Other Parts Discussed in Thread: USB2ANY
Hello,
I am trying to Start and verify basic functionality of BQ79600EVM with USB2ANY and BQAutoEval
1. BQ79600EVM-030 is with default settings 5V/UART (will switch to SPI afterwards). BQ79600 is still not connected to BQ78718, etc.
2. USB2ANY - software installed successfully upgrade to last hex file. J4, mid connector is used.
3. BQAutoEval installed (should I install also cloud agent, driver package for TDS). I cannot choose USB2ANY as communication port, even it is present in the control panel.
4. No external power supply for now (J4 has no possibility to output 5V?)
5. USB2ANY connected to BQ79600, connect seems OK, UART interface chosen and it seems like 5V on&off is working fine (no any LED indication on BQ79600 board)
However I cannot see anything from BQ79600 registers, etc. ..I found several documents for linking BQ79600, USB2ANY and BQAutoEval and it is a bit confusing?
Can you please give&explain basic sequence to get this evaluation chain up and running to verify basic functionality (even just reading registers of BQ79600)?
Thanks in advance!