This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR33640: Method of determining parameters

Part Number: LMR33640


Hello team,

I received a question from the customer.

Could you please explain the calculation process for the highlighted areas?

VIN:***V,VOUT:***V,fsw:***kHz,K:***,IOUTmax:***A

For example, the following calculation results in L = 13.9uH.

where, VIN:30V,VOUT:5V,fsw:400kHz,K:0.3,IOUTmax:2.5A

Regards,

Masa