Posting for a customer:
- When using a boost configuration for RGB LEDs with the LP8866, what is the recommended way to account for the Vf being different on RGB? Can they provide a description of what is typically done?
- Another way to ask it is, what is the range of the 6 current sources? How much Vf difference can they adjust to and how much power can they handle?
- On the LP8866, does the PWM input need to be used for dimming or can this be handled by I2C commands?
- What is the recommended way to do a hardware reset on the LP8866? Is there a I2C command to accomplish this? Or is control of the enable needed?
Can you help us out here ? We need a quick response if possible.
We are using this TI chip to drive between 38 to 40 RGB LEDs using I2C protocol.