According to the datasheet, when the output voltage(Vo)
of PTH08T230W is set to 1.0V, the maximum input voltage is VoX11, so the maximum input voltage is 11V. But in sltu003, the input voltage is 12V. I want to know if 12V input voltage can be used on PTH08T230W to get 1.0V Vo?