-
Help the customer review the schematic design, the inductance is 0.22uh 0.8 mO
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Help the customer review the schematic design, the inductance is 0.22uh 0.8 mO
Hello,
I will post my answer later this week or early next week.
Regards
Hello, here is my comment so far and still reviewing:
1- VR_ON pull up to 3.3V is 10K and pull down is 2K. Vvr-on = 2K/12K*3.3V = 0.55V. It is higher than VR_ON max ViL
2- pull ups for VCLK, nALERT and VDIO are not in this file. Are they somewhere else?
3- Feedback signals VR_PVNN_NAC_VSENSE_DP and VR_PVNN_NAC_VSENSE_DN are only shown in this file. Are they somewhere else?
4- Remove R4360 pull up for B-RAMP. Check the table
Hi Xiaofu,
I did not understand your above question. What inductor you mean?
Regards