Hi all,
I have a couple of doubts about the TPS552882 datasheet:
1) I have used WEBENCH for a first design, and for my specifications (Vin ~ 14V-26V, Vo = 20V, Io = 1.5A) WEBENCH tells me that the design is unstable when trying to modify the switching frequency. I can only achieve a proper design with 300kHz and 600kHz, but nothing in between, which gives me almost no flexibility in my inductor design. For 300kHz (which gives me the highest global efficiency), the inductor that I chose is 15uH and the resulting peak-to-peak inductor current ripple would be around 1A (@26Vin), which is around 68% of the nominal current. I have two concerns here: the inductor's size (which I could reduce sacrificing a bit of efficiency) and the recommended operating table (section 6.3 in the datasheet) in which the maximum "Effective inductance" is defined as 10uH. Could I then choose a 15uH inductor or would it affect somehow the performance of the converter? Also, for such low current specifications, I have calculated that I only need around 7uF effective capacitance in both the input and output of my converter, but this value is smaller than the minimum recommended Cout (10uF). Would it be really a problem?
2) Regarding the internal LDO for VCC, I was wondering which is its typical current consumption. I'm trying to evaluate weather or not implementing an external voltage rail to supply VCC, but I must calculate the losses in the LDO beforehand. Could anyone provide this information?
Thank you very much for your time!
Best regards,
Juan