This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59116-Q1: I use eight TLC59116-Q1 chips to control 128 lights individually, The first question: Can the output of each circuit of the chip be adjusted from 5mA to 120mA? 2. If 20 lamps are lit at the same time, whether the current of these 20 lamps ca

Part Number: TLC59116-Q1

I use eight TLC59116-Q1 chips to control 128 lights individually,

The first question: Can the output of each circuit of the chip be adjusted from 5mA to 120mA?

2. If 20 lamps are lit at the same time, whether the current of these 20 lamps can be different, such as 120mA, 50mA and 10mA