Hi Team,
Can you please help find a wireless BMS for the specification below?
Wireless Power Bank
• 15W wireless Tx for QI compliant Rx
• 25W PD & QC 4.0 Fast Charging
• 3.5 hours power bank recharge time with USB-C & PD
• Simultaneous Charging 15W+25W
• Smart LED Indicators to show battery status
• 30,800mAh battery capacity
• Built-in intelligent chip to protect devices against overcharge, over-discharge, excessive currents, short circuits or overheating
• 4 output and 2 inputs ports
4 outputs = 2x type A ports + 1 type C + 1 Micro B
Not Micro B instead fourth one is wireless.
2 inputs = 1 type C (same that is used for output) + 1 micro B
Something similiar to IP5328P with wireless option added if possible
if possible send a reference design with suggested solution if there is any
Thank you kindly,
Regards,
Marvn