This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS73801: temperature caculate

Part Number: TPS73801


Hi,

I would like to know how to caculate TPS73801 temperature diff.

If Vin=19V, Vout=5V, 300mA, may cause (19-5) * 0.3 = 4.2W power dissapation on TPS73801.

If using RθJA = 50.5°C/W, it may cause 4.2*50.5 = 212.1 °C rise on TPS73801?

It is over TJ= 125°C limitation. it seems strange, or something I missed?

Thanks!

Jeff