Hello,
I see that ff [LEDCHG] = 1, the LED display will show the state-of-charge during charging when Current() > Charge Current Threshold. Is there a way to keep the LEDs on once charging has completed and the charger is still connected? Can this be done with the LED TOGGLE MAC command maybe? I don't see it in table 13-1 to say if it's available in SEALED mode.
Thanks,
Michael