Hello,
I have designed a circuit that includes BQ24780S IC. My schematic design is almost same with evm module but according to TI Forum I have changed somethings like BATFET and RBFET. TI supporters said these are any effect on working. When I plugged the DC Power supply, I can communicate with IC via SMBUS. My measured values are valid according to evm. But when I set the ChargerVoltage() and ChargerCurrent, There are no gate drive pwm. Both side, HIGH SIDE MOSFET and LOW SIDE MOSFET. HISIDE MOSFET gate is always 0.8V and LOSIDE MOSFET is always LOW(0 Volts). Why I can not see gate driver PWM's? My Charger out is the same with HISIDE MOSFET GATE Signal, 0.8V.