This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61220: current requiremen

Part Number: TPS61220


Hi Experts,

I am posting this on behalf of the customer. Here are the full details of the inquiry below.

I'm using the boost converter TPS61220 and I have a load current requirement of 100mA
in the datasheet, it is given that it can go to 100mA but when I'm trying to design it in the webench designer with my required voltage levels, it shows that the maximum is 15mA only my input voltage level is 3.3V and the output voltage is 5V so will it work for that current or should we go for another component?

I have drawn one schematic just need confirmation if it would work find for the given rating:

Vin = 2.5 to 3.5 V ( 3.3 Nominal)

Iout= 100mA

Vout=5V

I have attached the schematics in JPG format in attachment.

 

Thank you in advance for your support.

Best regards,

Jonathan