Other Parts Discussed in Thread: TPS51200, TPS53915, TPS546A24A
Hi Experts,
I am trying to help on of our customer with the below concern:
He has a project have to drive DDR3/4 DRAM on board and require PMBUS control
He already found part for VDD, now he needs parts for VREFCA/DQ, VTT and VPP
Do we have any parts provide
VREF,VTT 0.5~0.9V with 1% tolerance, 5mV step, min 0.75A, PMBUS control
VPP 1.5~2.8V, 5% tolerance, 10mV step, min 3.75A, PMBUS control
Upon checking, we do not have a DDR memory power IC that can fit his requirements. I have filtered our list of devices considering the below parameters:
DDR memory type: DDR3, DDR4
Output: VTT, VREF, VPP
Now, we also thinking of a DC/DC step down regulator but not sure what will fit. May we ask for your assistance on this? Thank you in advance.
Best regards,
Gerald