This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61500: As Backlight for 5 LCd's

Part Number: TPS61500

Hi, TI Support Team

I want to drive 5 LCDs (EA TFT020-23AI), that require 24V, 20mA each. I have the circuit from the datasheet and I get about 24V, so far so good. But on LED+ there are synchronously with Fs noises of 2.5V. These fluctuations cross-talk on the SPI communication and interfere with the writing to the LCDs.

What can I do to reduce these fluctuations?

Thanks