This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CSD16340Q3
CSD17556Q5B
CSD25402Q3A
CSD86350Q5D
CSD87333Q3D
CSD25402Q3AT
CSD16340Q3T
CSD17559Q5
CSD17556Q5B
CSD13202Q2
CSD13202Q2
Hello Chaohsiang,
Thanks for your interest in TI FETs. Please see table below with the ESD passing voltages for the list of FETs you provided. The CSD25402Q3AT and CSD16340Q3T are the same FETs as the non-T part numbers in a smaller reel size.
|
|||
Product Code | HBM Pass Voltage | CDM Pass Voltage | |
CSD13202Q2 | 350V | 1500V | |
CSD16340Q3 | 150V | 2000V | |
CSD17556Q5B | 2500V | 2000V | |
CSD17559Q5 | 2500V | 2000V | |
CSD25402Q3A | 750V | 2000V | |
CSD86350Q5D | 500V | 2000V | |
CSD87333Q3D | 3000V | 2000V |
Best Regards,
John Wallace
TI FET Applications