This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A47: noise performance across Output Capacitor

Part Number: TPS7A47


Hello team,

My customer has a question about noise performance vs Output Capacitor value.
Would you please share the noise performance in case of Cout = 10uF case?
 

In ds, the following is described.
8.2.2.1.1 Input and Output Capacitor Requirements
The TPS7A470x is designed and characterized for operation with ceramic capacitors of 10 µF or greater at the
input and output. Optimal noise performance is characterized using a total output capacitor value of 50 µF. Note
especially that input and output capacitances must be located as near as practical to the respective input and
output pins.

When the output capacitor is 50uF,  the noise performance would be better. But The customer would like to use smaller capacitor. So he would like to know the noise performance in case of Cout = 10uF case, or comparison between 10uF and 50uF. Would you please share?

Best Regards,
Akihisa Tamazaki