I have some questions about BQ27426:
1. What are the functions of the maximum analog rate and the minimum analog rate? Do users need to set?
If setting is required, how to evaluate the reasonable setting range? If the default value is used, what is the basis for setting the default value?
2.Whether the two parameters of Trace Resistance and Downstream Resistance need to be set by the user?
If user setting is required, how to evaluate the setting range? What is the basis for setting the default value? If possible, please explain the specific functions of these two parameters in detail?