I designed a device for automotive purpose and use LM5060 as a high-side protective chip.
But during the design stage, I find out some weird phenomenal.
- the chip's output will be determined by the slew rate of the input voltage from 0V to 27V.
- but when the input voltage goes down to around 13v, then the slew rate of input voltage will not have any impact.
below are some of my test steps:
- I at first set the power bench's output voltage to 27 and then shut down the power bench totally.
- connect the output port of the power bench to the input of the LM5060.
- turn on the power bench.
- because it will take around 350ms for power bench's output reach 27v, so I will see the output of the LM5060 can be generated normally.
- I then keep the output of power bench on with 27v output.
- then disconnect the cable between power bench's output and the input of the LM5060. Wait for minutes for lm5060 to totally discharged by capacitor.
- I then plug in the connector so that the 27v will apply to LM5060 direclty.
- under this situation, I cannot get the LM5060 generate output voltage.
- However, the same two test on 13v is normal. Which will generate output voltage by lm5060.
Would be appreciate if someone can help me figure out what's wrong with my design.