Other Parts Discussed in Thread: TINA-TI
Hi I am design an inrush circuit as shown in the image. The voltage is 3.3v (QSFPDDPLUG33 and QSFPDD33). Can the circuit work?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi I am design an inrush circuit as shown in the image. The voltage is 3.3v (QSFPDDPLUG33 and QSFPDD33). Can the circuit work?

Hello David,
Thanks for your interest in TI FETs. I am assuming the input is QSFPDDPLUG33 and the output is QSFPDD33. Is that correct? I created a simple TINA-TI simulation (attached), left out the ferrite beads and schottky diode and increased the value of R585 to 1MΩ. Please see below. I applied a 3.3V ramp with a rise time of 10μs and it seemed to work OK. Let me know if you have any questions.


Best Regards,
John Wallace
TI FET Applications
Hi John,
Yes, you're correct. The input is 3.3v QSFPDDPLUG33 and the output is QSFPDD33. The simulation looks good. One question is about value of R1 (R585), 1MOhm. It's very large value kind like open circuit. What would happen if I do one of the following:
1. Remove R585 completely. Or
2. Lower R585 to 100K or 10K
Thanks,
David
Hi David,
R585 pulls the gate up to the source to make sure the FET is off at initial startup and also forms a resistor divider with R576. I sized it at 1MΩ to minimize the current flow thru the 2 resistors while maximizing VGS to fully turn on the FET. I would recommend keeping the resistor and not reducing to less than 100kΩ.
Thanks,
John