Other Parts Discussed in Thread: CSD18540Q5B
Hi Team,
According to our customer the Webench proposed design does not align with the real PCB design. He built the PCB and tested the board. Please see his findings below.
1. The efficiency of the device drops in the actual PCB by 7%. The PCB layout is the generated design in Webench.
2. If the output current is 19A, the Webench recommended two parallel CSD18540Q5B MOSFET but if the output current is set to 20A only one CSD18540Q5B MOSFET is recommended.
3. The efficiency of the device is lower using two MOSFETs compared to a single MOSFET by 2% and both doesn't meet the efficiency in the Webench simulation
Here is the Webench design file
The specifications are:
Vin = 30V
Vout = 5V
Iout = 20A
Please see attached excel file from our customer.
What could be the caused of this error?
Regards,
Danilo