Other Parts Discussed in Thread: TPS25820, TUSB564
Hello
For a new project we want to implement USB-C with Displayport ALT mode.
We have used the Toshiba TC358867XBG in another project, which makes 2-lane Main Link and AUX channel.
Currently this project uses 3 cables (Displayport, Power and USB2.0) but we want to have the advantage of USB-C and have USB, Power and Displayport over 1 cable.
So we want to connect this to the TUSB546 redriver and TPS25820 controller.
I think it should work but I am just a bit lost on how to connect everything.
The Toshiba chip has just 2 Lane Displayport and we are using USB 2.0(so these will go straight to the centre pins of the USB-C connector).
The TUSB546 has several options but which one should I configure?
We don’t have USB3.1 and only 2-Lane Displayport, but this option isn’t available.
Do I need to configure it as 4-Lane DP and don’t connect Dp3 and Dp4 on the TUSB546?
Or configure it as One Port USB3.1 + 2 Lane Dp and don’t connect the SSRx and SSTx.
And what do I need to do with the SSEQ pins when I don’t have USB3.1?
Can I configure them to the lowest gain?
I planned to use the TUSB546 in GPIO mode.
The TPS25820 will control the flipsel with the POL pin and the SINK pin will control the CTLSEL pins.
I have ordered the TUSB546 and TUSB564 kits so I can do some testing but it will take a while for them to arrive.
Would be great if you could help me a bit further.
And is it possible to have the schematics checked before I start working on the PCB?