Hello.
I want to use BQ76PL356 to monitor ultracap charges.
4 cascaded BQ to control up to 24 cells.
BQ76PL536 is able to disable protections, and I can control the charge of the suparcaps (initially discharged) usign external hardware and when supercaps get the minumum recommended voltage BQ76PL536 would begin to manage them.
Usually all related examples take the power supply for the BQ76PL536 directly from the cells. But if I manage discharged supercaps there is no voltage to supply.
¿Can I use an external power supply?.
If so, please let me know how I need to connect the external power supplies to the four BQ76PL536 cascade connected.
I suppose I should connect isolated power for each BQ76PL536, connecting possitive to BAT and negative to VSS................... need the external power supply to be higher than the maximum voltage that could reach all the cells connected to BQ76PL536?.
Last question:
I´m not able to see clear differences between BQ76PL536 and BQ76PL536A.
Is the accuracy the main advantage of the BQ76PL536A?. Or............ are there other interesting advantages to take care about?.
I´m not sure if I should push BQ76PL536A instead of BQ76PL536.
thabks and regards