Hi team!
The customer want to use TPS63802 to output maximum power, but they are not sure whether the device can work normally when the ambient temperature is 0~75 degree centigrade and output is maximum power. At the same time, how would we do the thermal design, what the temperature is the device and how to calculate the temperature ? Is there any design need to be emphasize?