Hardware design, in the configuration of dog feeding time, how to consider? If the configured feeding time is too short (in order to meet the requirements of FTTI), the feeding time will arrive before the system is started. As a result, the system cannot be started. If the configured feeding time is too long (in order to meet the startup time requirement, but much longer than the FTTI time), although the system startup time requirement is met, the FTTI requirement cannot be met.