This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54294: TPS54294PWP

Part Number: TPS54294

In our circuit, we are generating 5V & 3.3V outputs by giving input voltage 7V. Same circuit is working fine with P/No:TPS542941PWP but when we replace with part:TPS54294PWP it is not generating the output voltage-5V.

The difference in functionality we observed are,

1. By increasing input voltage gradually TPS54294PWP IC is not generating output voltage till 10V. Observed at 4V the output voltage is increasing from 0V to 2V & then again decreasing to 0V. At this time some humming noise observed from the IC. If we make power-supply On/Off by increasing the input voltage, then at 7.5V it is generating 5V o/p.

2. Also observed when we keep any conductor/measuring probe on VFB1 & VFB2 pins then the Output is getting decreased from 5V to 0V.

Please let me know the difference between these two parts P/No: TPS54294PWP & TPS542941PWP & why i am not getting the output voltage 5V.