Part Number: LP5912
I have one question.
The LP5912 is used to change a voltage from 3.8V to 1.8V.
1.8V is supplied to the external IC from the LP5912.
A maximum rush current of 1.4A flows for 20us when the external IC starts.
Is there the LP5912 at risk of being broken by 1.4A rush current for 20us?
I send the waveform of the rush current.