Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5157EVM-SEPIC: LM5157EVM UVLO Resistor Divider Selection

Part Number: LM5157EVM-SEPIC
Other Parts Discussed in Thread: LM5158, LM51581

I have a modified LM5157EVM SEPIC with an LM51581 where the Bias if fed by the input and output through diodes (J6 1-2, J7 1-2).  I would like a turn on at 6V, and a turn on at 2.24V. My UVLO resistor divider consists of a 68K and 22K based upon the LM5158 SEPIC Controller Design tool.  This divider results in a turn on of approx 6.2V, while the turn off is at 5.6V. 

What am I missing?

  • Hello Raymond,
    Thanks for reaching out to us via e2e.

    The UVLO input has a hysteresis of 50 mV between rising and falling edge, to avoid oscillations.
    The quick start calculator is making use of that and offers you a calculation to tweak the hysteresis on the input voltage a little bit,
    dependent on the resistor values.
    To make this clear: This is NOT meant to give you full freedom for a big delta between the on and off voltages.

    Your calculation somehow went wrong.
    When I enter 2.24V and 6V, I get 712K and 237K as a result.

    So I end up with an overall resistance which is close to 1 Megaohm.
    I am pretty sure that the system would no longer work stable, when you go above maybe 200K or 300K.

    And this is what I meant to say earlier on.
    This concept with the small hysteresis is meant to avoid oscillations, not to allow for such a big delta between on and off voltages.

    Best regards,
    Harry

  • Hello Raymond,

    I have not seen an update from you for two weeks, so I assume the questions are answered and the issue is solved.
    I close this thread now. If there is still something open, please reply and the thread will get opened again.
    If you have any other question or of the thread has been locked, please open a new one.

    Clicking the Resolved Button also helps us to maintain this forum.

    Best regards,
    Harry