This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

any solution to support dual DC input PSU

Customer was asking for the solution to meet the below requirements

1. Dual input source

1)  9V~60VDC

2) -38.4V~-72VDC

Need to support one source switching to another one, without damaging the system

2. Vout=12V 

3. Output power level: 70W

Could you please help suggest any solution? Thank you.