This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5156: Isolated DC/DC converter for PoE

Genius 17425 points
Part Number: LM5156
Other Parts Discussed in Thread: LM5155

Hi Experts,

Can you confirm if the design from Webench:

https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=3684E099BCEC689E

Can be used by customer for the isolated DC-DC converter for the Power over ethernet application and to meet the timeline need a component with a schematic.

Below are their requirements:

Boost converter with isolation
Input Voltage: 12 to 36V
Output Voltage: 48V
Output Power: 19W

Application: Power over ethernet (POE): Power Sourcing Equipment (PSE) up to 19W - IEEE802.3af

Thank you.

Regards,
Archie A.