This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65381A-Q1: 1.2V output cap selection

Part Number: TPS65381A-Q1

Hi,

Customer's Spec is as below.

Vin 12V, Vout:5V / 50mA(for CAN transciver), 3.3V / 50mA ( for C2000 F280025), 1.2V/ 10mA( for F280025 reference).

Customer schematic is as below.. Do you help to check it? Do you have any suggetion for 1.2V(VDD1) output cap? The EVM schemtic is  22uF.

Thanks & regards,