Good Morning,
I am working on BMS that's requires high coulometric measurement accuracy, two battery IC monitor devices (Bq27010) and Bq26220 (21)) sould be implemented. I would like to have further information about:
Bq27010: Relation between the output conversion (MicroVh) and input voltage developped across the sense resistor How to estimate the overall accuracy of the output data (unit : microVh), including the following information: fOSC Internal oscillator frequency -2.2% 1.5% Current gain variability -0.5% 0.5% Coulometric gain variability -1.7% 0.5% Coulomb counter input offset(1) -15 0 15 μ
V How fast fully conversion can be performed between the initiated of the input signal conversion and the output data (coulombs couting) => Delta sigma latency (is second)
do you have any suggested solution for
high coulometric measurement accuracy using other bq ?
Best regards
Thank you very much