There seems to be a typo in sec 3.8 of TRM for -r2 firmware. It says 32.76mAh. However, the Design Capacity max value mentioned in Table 7-1 is 32767mAh (which makes sense for a 16-bit signed register). Hence it should follow that in sec 3.8, the value should be 32767mAh or 32.76Ah (the value up to which the scale factor can be 1). What am I missing here?
By the similar logic, in sec 3.8, are power and energy values also wrong?
Thanks