This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563202: Test reports for TPS563202

Part Number: TPS563202

Hi team, 

I am using TPS563202 for 5V 2A power supply in my design. I am not able to find the simulation file (Spice model) for this TPS563202. It will be very helpful, if you provide the simulation file or spice model for TPS563202. In case simulation is not available, please provide me the test case with test results which includes start up, steady state, load transient, input transient and along with resistance tolerance variation.

Thank you& Regards,

KAKI POTHURAJU