HI team,
There are no VLDOIN and also VOUT1,2 ABS max in the datasheet. How much is the ABS max?
Regards,
Hayashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI team,
There are no VLDOIN and also VOUT1,2 ABS max in the datasheet. How much is the ABS max?
Regards,
Hayashi
Hi Jimmy,
When customer sets 20V as output voltage by resistor divider with its typical value, the output voltage might be higher than 20V by resistor accuracy. In this case, what will happen?
This is similar question, what will happen in setting >20V in resistor?
Best regards,
Hayashi
Hi Hayashi,
There shouldn't be an issue with setting the output voltage a bit higher than 20V.
However given that the 2.2uH inductor is integrated into the power module, this may limit low low of a frequency you can go before device either has insufficient slope compensation or hits current limit.
For a 20V output application, I would suggest operating at 28V input and switching frequency starting at 1.2-1.4MHz.
Regards,
Jimmy