This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: Maximum number of reflow cycles

Guru 21045 points
Part Number: TPS25750

Hi Team,

 

Could you please let us know the maximum number of reflow cycles of TPS25750DRJKR(WQFN PKG)?

 

Regards,

Hide

  • Good Morning,

    I will review our documentation and get back to you by EOB March 3rd.

    Kind regards,

    Conner Gillette

  • Page 68 of the attached TPS25750 data sheet (tps25750.pdf), table “Packaging Information”, header “MSL Peak Temp”, lists the device as “Level-2-260C-1 YEAR”.

    The last line of Section 5 of the attached MSL Ratings and Reflow Profiles document (spraby1a.pdf) states “The IC packages are classified according to J-STD-020 and withstand three reflow cycles.

    Additionally, please take into consideration the below information when performing additional reflow soldering:

    The last paragraph of Section 2 of the MSL document states “For IC products with MSL Rating 2 and lower, the floor life needs to also be considered after a first reflow soldering process. Moisture from the environment where the boards are stored will ingress into the package. A bake of the assembled board may be required prior additional soldering process steps, Rework steps and other process steps with temperatures above the local water boiling point.

    tps25750.pdf

    1172.spraby1a.pdf

  • Hi Conner-san,

    Thank you for the detail information.

    I greatly appreciate your cooperation.

    Regards,

    Hide