Hi team!
The customer wanted to use about below 1Mohm resistor as feedback resistor. Because the selected resistor type is almost below 1Mohm. But as datasheet said, we suggest the feedback resistor is as shown below. The customer needs to keep low voltage output ripple(about 30mV) and the output is 5V~7V, about 10mA. If they choose resistor below 1Mohm, what is the risk? And do you have any advice?