Hi team,
When I test on BQ25601, I can see REG07 BIT[7] is set to 1 and the input current limit is set to 2.4A at start-up period. But when I set the current limit to another value, then lower the input voltage to 4V and increase it back to 4.5V, the input limit is set to 2.4A again. This is weird because the input current limit detection is only applied in start-up period. I can see the charger is in VINDPM status but the chip did not shut down so the detection should not be applied when the input voltage rise from 4 to 4.5. But when I set the VINDPM to other value(default 4.5V), for example, 4.2V or 5V, the input current limit would not be reset. Can you help to check on this?
Test condition:
input voltage: 4.5V - 4V - 4.5V
battery voltage:3.8V
turn off watchdog timer
Others are default value.
Best Regards,
Peter