Other Parts Discussed in Thread: BQ25616, , BQ24251EVM-150, BQ24251
One customer is considering bq25243, USB Type-C and Li-Ion battery.
When both USB and Battery connecting, /PG was not assert Low and charge current become about 100mA in any EN1 and EN2 setting.
(RLIM = 300Ω = 1000mA, RSET = 270Ω = 833mA)
Please let me know about two points below for D+ and D- detection.
①Is there reason and improve idea?
I think there is a problem with detection of D+ and D-.
By the way, Battery condition is 3.5V (not become dead battery), EN1 and EN2 toggle is delayed 1sec after USB insert.
②About condition for USB insert and EN1 and EN2 are not toggle, D+ and D- detect was differed on battery connect and no connect.
Are above operation normal or D;/D- detection error?
・Battery is not connect, USB is only connect (Normal)
D+ pin: USB insert → 5V (about 110ms) → continue to 500mV
D- pin: USB insert → continue to 500mV on the same timing for D+ become 500mV
・Both Battery and USB are connect (Abnormal?)
D+ pin: USB insert → 5V (about 110ms) → 500mV (about 200ms) → changed to low
D- pin: USB insert → 500mV on the same timing for D+ become 500mV → changed to low
Best regards,
Satoshi