Hello,
My customer reviews to use LMR51430 under the following conditions.
- VIN = 10V~30V, VOUT = 9V, IOUT = 2A
They calculated the expected Tj for the worst-case temperature with the formula below.

Ta = 85℃, RθJA = 107.8℃/W, Power = 9V*2A = 18W
In this case, this device cannot be used because it exceeds the allowable Tj specification.
1. Is the Tj calculation above correct? What is the maximum ambient temperature allowed for 9V@2A with this device?
2. Can you please recommend a DC/DC converter product that can be used at a higher ambient temperature for the customer's VIN, VOUT and IOUT?
Thank you.
JH