Hi,
Customer wants to recharge the supercapacitor by applying BQ25173.
Please review the schematic.
FAST CHARGE CURRENT 0.3A / VREF 3.52V

Add, customer's question.
Q1 : VUSB not connected (IN = Floating), SUPERCAPAICTOR (Out = 3.6V) conditions
/CE pin Low - Quiescent current? /CE pin High - Quiescent current?
Q2 : Why is there a current difference between connecting the bottom resistor of FB with GND and connecting it with /PG, and what is the current difference?
Q3 : For /PG and STAT, I would like to get the following input from the HOST with pull-up. Is it possible?
- /PG : USB Detect
- STAT: Charging, charging complete.