Hi team,
My customer needs to know our light load efficiency data. Could you please help to test according to the excel data?
The part number is LMR43610RS3QRPERQ1, PFM, Fsw=400k.
Thanks for your support!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer needs to know our light load efficiency data. Could you please help to test according to the excel data?
The part number is LMR43610RS3QRPERQ1, PFM, Fsw=400k.
Thanks for your support!
Hi Iris,
Sorry for the delay. Here is a quick update to let you know that we have not forgotten this case. We have assembled a setup able to measure efficiency at micro ampere load, and we also found an EVM and also swap the IC with an LM43610 and tested according to customer's load conditions. However, the IC variant in hand sets the frequency to 2.2MHz. We are getting the variant able to set the frequency to 400kHz and will re-test. I believe with the oscillator sets to 400kHz, the IC would draw less current and result in higher overall efficiency. The IC should come early next week and we should be able to share the results soon.
Thanks,
Youhao
Hi Iris,
Again, we apologize for the delay. Attached is the efficiency results. Note that the EVM inductor is 3.3uH, for both 3.3V and 5V output settings. If the customer's load is always light, a higher inductance should help increase the efficiency slightly higher.
LMR43610 light load test--400kHz 3p3uH.xlsx
Hope this helps.
Best Regards,
Youhao