This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22925: Overload/Short condition

Part Number: TPS22925

Is the TPS22925C current limited or thermally protected? What happens when I overload/ short the output of this part to ground? Potential application would be to power a chip that will draw about 200mA on a 1V rail. The device is connected in series with a 1V supply and the other chip; the 1V supply is capable of high current so it could damage the TPS part if the TPS output is shorted to ground.