Team,
my customer is looking at dissipating 3.3W from this LDO on a 4layer 1oz copper FR4 : I believe this is the same stack up as the EVM : what temperature elevation can they expect?
Olivier
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
my customer is looking at dissipating 3.3W from this LDO on a 4layer 1oz copper FR4 : I believe this is the same stack up as the EVM : what temperature elevation can they expect?
Olivier
Hi Olivier,
The thermal performance that they get on their board will depend on the layout they use. If there is a lot of same-side copper, via connections to internal layers of more copper, and ideally more copper on the bottom layer, then they can reduce the datasheet thermal metrics by around 30-40%. So with a more thermally optimized board layout like this, they can expect a junction temperature rise of about 41.8C/W * 0.7 * 3.3W = 96C to 41.8C/W * 0.6 * 3.3W = 82C.
Are they dissipating 3.3W in the LDO to drop the voltage or is the LDO delivering 3.3W to its load?
Regards,
Nick
heloo Nick, You got it right : the 3.3W is the power dissipated in the LDO. thanks