This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Michael,
Your understand is correct, so is your customer considering the supply current for their application?
Besides, I'm curious about why customer choose LP55281, is it because they need the boost function?
If the boost function and Audio Sync function is not necessary for their application, I recommend LP5012 for them, it will be cheaper than LP55281.
Thanks!
Ives.
Hi Ives,
Thank you for the information. They want to use LP55281 because the Iq is lower than LP5012. Do you know what that's the case? LP5012 is much newer so I'm surprised it's so much more power hungry.
Also, if we're not using the boost function of LP55281 and instead using an external supply, should SW and FB be grounded or left floating?
Thanks,
Michael
Hi Michael,
If the boost function is not used, please left it SW and FB floating.
But if the boost function is not used, I still suggest you with LP5024.
With new device we can provide better support and the cost is lower than LP55281.
Besides, LP5024 is much easier to use.
Please consider my suggestion and recommend LP5024 to customer .
Thanks!
Hi Ives,
Customer wants to use LP55281 because the Iq is significantly lower. Why is the Iq of LP55281 so much lower than LP50xx?
Thanks,
Michael
Hi Michael,
Even the Icc value in datasheet shows difference between two device,but I think it is not the main power consumption during the application. So it will not show big different for them,but if use LP50xx,their cost could be much lower than LP55281.
Thanks!