Other Parts Discussed in Thread: TPS793, TPS7A20, TPS7A10
Hi team,
Do we have some P2P solution for the TPS79318YZQR?
Thanks.
BR
Mason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Mason,
I would recommend looking at the TPS7A2018PYCKR these are similarly small in size, not p2p, but improved performance.
Another one to look at is the TPS7A1018PYKAR, this is the same package, but different pin out.
TPS793 | TPS7A20 | TPS7A10 | |
AEC Q100 | NO | NO | NO |
Output Options | Adjustable Output, Fixed Output | Fixed Output | Fixed Output |
Iout (Max) (A) | 0.2 | 0.3 | 0.3 |
Vin (Max) (V) | 5.5 | 6 | 3.3 |
Vin (Min) (V) | 2.7 | 1.6 | 0.75 |
Vout (Max) (V) | 5.4 | 5.5 | 3 |
Vout (Min) (V) | 1.22 | 0.8 | 0.5 |
Fixed Output Options (V) | 1.8, 2.5, 2.8, 2.85, 3, 3.3, 4.75 | 0.9, 1.05, 1.2, 1.5, 1.8, 1.825, 1.85, 2.2, 2.4, 2.5, 2.7, 2.8, 2.85, 2.9, 3, 3.1, 3.2, 3.3, 3.6, 4, 4.2, 4.5, 5, 5.5 | 0.6, 0.8, 1.05, 1, 1.1, 1.2, 1.5, 1.8, 2.5, 2.8, 3 |
Enable | YES | YES | YES |
Power Good | NO | NO | NO |
Output Capacitor Type | Ceramic | Ceramic | Ceramic |
PSRR @ 100KHz (dB) | 44 | 60 | 36 |
Noise (uVrms) | 32 | 7 | 110 |
Accuracy (%) | 2 | 1.5 | 1.5 |
Vdo (Typ) (mV) | 112 | 110 | 70 |
Iq (Typ) (mA) | 0.17 | 0.0065 | 0.0016 |
Thermal Resistance θJA (°C/W) | 178 | 179.1 | 169.4 |
Min Package Area (mm2) | 0 | 0.379456 | 0.8814 |
Package Type | DSBGA, SOT-23, SOT-23 | DSBGA, SOT-23, X2SON | DSBGA, WSON |
Thanks,
McKyla