Part Number: TPS62933EVM
Other Parts Discussed in Thread: TPS62933
Hi Expert,
Good day.
The customer needs your expertise. Please advise.
my name is Raffaele Salvati, a Ph.D. student at the University of Perugia. I am working on a WPT system for industrial equipment for dynamic applications and currently using your TPS62933EVM as DC/DC Converter module.
Due to the application scenario, we cannot transfer power continuously, therefore we decided to use supercapacitors as storing devices after the DC/DC (due to their low voltage rating). The system is able to charge the capacitors and supply the load with 5 V but using an Arduino to monitor the supply voltage I found out that there are several spikes of about 1 V.. I think its due to the transient response of the DC/DC and tried to fix it adding the feedback capacitor but I encountered a few obstacles.
First of all, I don't know how to define the output current since the load (parallel of supercapacitors and an Arduino board) varies depending on the capacitors' charge status. However, assuming a Resr of the output capacitor close to 0, I calculated that using C0 = 2.5 F the minimum feedback capacitance is 390 uF ("Stability Analysis and Design of Internally-Compensated Peak Current Mode TPS62933 - Part II: How to Select the Feedforward Capacitor", Eq. 18).
I will try this configuration next Monday, do you think this could solve the problem or there is something better I can do?
Keep safe
Regards,
Josel