Hey
I'm writing some programs for the LP55231 engines to create the following effect:

const uint16_t lp55231_program_Test_2_code[] = { /* Mapping Table location */ /* 0 */ MUX_LD_START(11), /* 1 */ MUX_LD_END(11), /* Engine One */ /* 2 */ SET_PWM(255), /* 3 */ END(0,0), /* Engine Two */ /* 4 */ MUX_SEL(LED_G1), /* 5 */ RAMP(RAMP_PRESCALE_0_488MS, 7, RAMP_UP, 255), /* 6 */ MUX_SEL(LED_G2), /* 7 */ RAMP(RAMP_PRESCALE_0_488MS, 7, RAMP_UP, 255), /* 8 */ MUX_SEL(LED_G3), /* 9 */ RAMP(RAMP_PRESCALE_0_488MS, 7, RAMP_UP, 255), /* 10 */ BRANCH(0, 0), /* Mapping Table*/ /* 11 */ RGB_ALL_RED, };