Other Parts Discussed in Thread: BQ79616, MSP430FR5994
Hi,teams
I want to use two development boards msp430fr5994 and BQ79616 for UART communication.
BQ device question:
I read from the data sheet of BQ79616 that its UART baud rate is 1MHz. I have two question for data sheet.of BQ79616
(1)Is 1M fixed? Can I set it to other baud rates?

(Note:I set the baud rate of msp430 to 9600Hz, I found that after connecting to 79616, the device cannot be addressed normally.)
(2)If the baud rate of the BQ device can be set to other values, why can’t it automatically address after I set it to 9600Hz?
msp430fr5994 launchpad question:
Now,I use two 430 development boards for UART communication. When the communication rate between the two boards is set to 9600Hz,
I can correctly read the value fed back from the slave and store it correctly, but when the communication rate is set to at 1MHz,
I cannot correctly read and store the value sent by the slave.
so,I want to now MSP430
(1)I want to know why I can't read the data correctly after the communication rate is increased?
(2)In the case of ensuring stable communication, what is the maximum communication rate of MSP430 UART