Part Number: LMZ30604
Other Parts Discussed in Thread: TPSM82864A
Hi,
My customer has the following requirements: Input voltage: 3.3V, output voltage: 0.9V, rated current: 4A, output voltage ripple :0.2% of Vout
My questions are:
1. Do we have a power module that meets this requirement?
2. Is this power requirement common?
3. If it is implemented with a converter, is there a recommended device or reference design?
Regards,
Charlie