This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP876242-Q1: Please recommend an IC with low output ripple

Part Number: LP876242-Q1
Other Parts Discussed in Thread: LP8764-Q1

Hi,

My customer has the following requirements: Input voltage: 3.3V, output voltage: 0.9V, rated current: 4A, output voltage ripple :0.2% of Vout

By interleaving and paralleling, do we have products that meet customer requirements? If not, please recommend a device that can provide as low output ripple as possible. Q1 or not-Q1 is fine.

Regards,

Charlie